stairs, escape route

Safe electrical installation in commercial and residential construction

Fire protection and lightning and surge protection from the ceiling to the roof

If we take a look at the interior of a building, then it soon becomes clear that electrical installations weave their way through it: starting in the cellar, through vertical shafts and corridors, up to the rooms which are actually used.

The risks from lightning strikes, surges and the spread of fire to the electrical building installation are frequently underestimated. Here, it is not only the direct lightning strikes that can lead to major damage to electronic devices and systems, but also lightning strikes at distances of up to two kilometres or even everyday switching operations in the power grid. Fires can also start quickly. Therefore, following the path of the current, suitable measures must be taken in the building to guarantee the safety of the people in the building and protect electrical devices.

Areas of fire protection

Block of flats
1
2
3
4
1

The cellar

2

The stairwell

3

The corridor

4

The vertical shaft

“The Circle,” Zurich

OBO ensures reliable cable routing in "The Circle", Zurich.

To Project
Swiss Life Arena Zurich

Bettermann AG takes to the ice at the Swiss Life Arena in Zurich

To Project
Mercedes-Benz Dealership

Mercedes-Benz car dealership

To Project
Montemor Tunnel in Portugal

Montemor Tunnel in Portugal

To Project

Fire protection solutions for every building type

With our comprehensive portfolio and decades of experience, we can offer the right fire protection system for every building. Why not convince yourself about our solution competence!

Tutorials

FAQ

On which regulations are the fire protection requirements based?

What are the different building types?

How do the fire protection requirements differ for different buildings?

Which protection aims are being pursued with the structural fire protection measures?

Which options do I have for fire-proof electrical installations in rescue routes?

Which fire resistance class must fire protection ducts in rescue routes have?

To what must I particularly pay attention with regard to underfloor ducts and trunking in the rescue route?

In the corridors of the building, there are installations above F30 ceilings. What must I take into account during installation?

You might also find this interesting

Gottfried Wilhelm Leibniz Library

Commercial and residential buildings

Education buildings

To equip education buildings with electrical technology for the future, individual technologies must be combined with centrally controlled systems. OBO offers the matching solutions for this.

Commercial and residential buildings

Office and administrative buildings

The world of work is changing continuously, as shown by open space offices. The OBO portfolio contains solutions for the electrical infrastructure that are discreet, flexible and reliable.

Commercial and residential buildings

Listed buildings

The monument protection is frequently at odds with the requirements for fire protection and lightning protection in buildings. Special solutions need to be found and OBO is happy to take on the challenge.

shopping centre, mall

Commercial and residential buildings

Shopping centres

Function and design, quality and long life: These are factors that are at the forefront of electrical installations in shopping centres. All these attributes combine the OBO solutions for this area.

corridor, doctor's surgery

Commercial and residential buildings

Healthcare

In hospitals, care homes and geriatric facilities, solutions from OBO secure a fault-free supply of power and data. They fulfil not only functional but also hygienic criteria.

Hotel Gallia

Commercial and residential buildings

Hotels and restaurants

Hotels, restaurants or congress centres – many people come together here, so that not only functional but also aesthetic requirements must be fulfilled. This is a challenge that’s tailor-made for OBO.

Warehouse, logistics

Commercial and residential buildings

Logistics buildings

Logistics buildings are characterised by expansive steel and concrete structures. To bridge large support spacings, OBO wide span cable support systems and heavy-duty vertical ladders are the ideal solution.

stadium

Commercial and residential buildings

Sporting and event locations

When thousands of people converge, nothing must be left to chance. This also applies to building infrastructure. OBO supplies reliable products, thus guaranteeing safety.

sofa, living room

Commercial and residential buildings

The construction of living accommodation

There is scarcely another place in which we feel as safe as within our own four walls. OBO offers a variety of electrical components for a safe and comfortable life.

Building, Glass

Construction industry

OBO solutions for commercial and housing construction

With many years of expertise and a comprehensive portfolio, we can ensure safe electrical installations in any building – from homes, to offices, all the way to hospitals and sports stadiums.

Contact

OBO Bettermann Export GmbH & Co. KG

Do you have any questions on this topic? We are glad to help!