Electrical installation for photovoltaic systems
Comprehensive protection, continuous availability, flexible installation
The procurement of a photovoltaic system (PV system) is always connected with a high level of investment, which should prove its worth as quickly as possible. This makes its continuous availability even more important.
What must you take into account regarding the subject of photovoltaics? As PV systems are installed on a roof or in an open location, they are particularly susceptible to lightning strikes and surge voltages. If the PV system is damaged, then the yield is lost for the duration of the repair work. In addition, extra costs are incurred, for example through the exchange of the inverter. It doesn’t have to be that way. With our OBO complete solution, you are sure to be on the sunny side. We offer not only a complete system for the lightning and surge protection of PV systems, but also future-oriented solutions for flexible installation: The Magic PV solution – reliable mounting systems for pitched and flat roofs and free-standing systems. With our innovative mounting systems for pitched roofs, flat roofs and free-standing systems, the installation of all standard PV module sizes is easier than ever. For more efficiency: Solar so good.
Long-lasting, reliable, resilient: warranty certificate for OBO Magic PV Solution®
We stand for quality: Our PV substructures are guaranteed to be free of material and manufacturing defects. In addition to the legal warranty rights, we also provide a voluntary warranty on metal and plastic components.

Your advantages at a glance
- Flexible mounting systems for pitched-roof, flat-roof and free-standing systems
- Complete system for almost any electrical requirements of a PV system
- Tailor-made support for the erection and operation of PV system solutions
- Long-term experience and competence connected with the protection and supply of PV systems
- System solutions for rapid and continuously safe installations
- Practical, comprehensive PV training courses
- Knowledgeable installation and planning aids
- Investment and legal security
- PV planning tailored to your individual needs and requirements with OBO Construct
System solutions
Smart PV planning – with the OBO Construct PV tool
With the OBO Construct tool for PV mounting systems for flat-roof and pitched-roof systems you plan your Magic PV Solution® tailored to your specific needs and requirements. Intuitive, clear, fast.
- Explained step by step
- Intuitive to use
- Order list created automatically
Good to know: Our aluminium parts are sourced exclusively from within the EU!
With OBO, you’re on the safe side when it comes to CBAM, the EU’s new climate protection tool, because all the aluminium parts for our systems are produced exclusively in the EU. Even the raw materials used come from EU member states.
No matter which PV system type you wish to implement, with OBO you can find the matching system solutions for the following areas of competence:
UniElektro PV system in Mittenwalde – a specialised solution without ballasting
OBO developed a special solution for the specific requirements of the roof construction: a ballast-free hybrid system comprised of Magic PV Flat Basic combined with UniBase Glue, which was bonded to the roof cladding.
Downloads
Solutions for photovoltaic systems
Magic PV Solution®: Mounting systems for photovoltaic systems
Project registration form Magic PV Flat
Project registration form Magic PV Field
Project registration form Cable management
Magic PV Flat Mounting times
FAQ
Which measures must I take to protect PV systems?
What do I need for the external lightning protection of photovoltaic roof systems?
How do I install external lightning protection in combination with a photovoltaic system?
How do I maintain separation distances to the lightning protection system in a photovoltaic system?
What options do I have for the strain relief of vertical cable routing in a photovoltaic system?
How do I best protect the inverter in a photovoltaic system?
How do I route cables in the area of emergency and escape routes with a photovoltaic system?
Who is responsible for correct protective measures in a photovoltaic system?
Can OBO solutions be combined with different mounting systems?
What documents are required for compliant planning?
What planning documents (CAD, tender texts, etc.) does OBO provide?
What test and approval criteria are relevant for PV systems?
Requirements
Taking responsibility, securing the system.
A wide range of standards and regulations must be complied with for the erection of a lightning protection system for a PV system. The erection engineer of the PV system is liable for correct fulfilment for 30 years. The requirements of the insurance company come on top of that.
The specialist company installing an electrical system is required by law to hand it over in perfect condition.
Responsibility of the operator
Through the feed-in of the gained energy, almost every PV system is subject to the requirements for commercial use. For the system operator, this creates the obligation, according to the accident prevention requirement BGV A3, to give the system the proper maintenance, checking and repairs.
These regularly recurring checks of the electrical system components must be carried out by an electrician.

Low-voltage electrical installations
- DIN VDE 0100-100 (IEC 60364-1)
- DIN VDE 0100-534 (IEC 60364-5-53)
- DIN VDE 0100-410 (IEC 60364-4-41)
- DIN VDE 0100-443 (IEC 60364-4-44)
- DIN EN 60664-1 (IEC 60664-1)
Commissioning test and documentation
- VDE 0100-600 (IEC 60364-6)
- VDE 0105-100 (EN 50110-1)
Requirements for PV power supply systems
- DIN VDE 0100-712 (IEC 60364-7-712)
- DIN EN 62446 (IEC 62446)
- DIN CLC/TS 61643-12 (IEC 61643-12)
- DIN CLC/TS 50539-12 (CLC/TS 51643-32, IEC 61643-32)
- VDE 0185-305-3 Supplement 5
Fire protection in the PV area
- VDE-AR-E 2100-712
VdS guidelines for fire protection and safety of electrical and photovoltaic systems
- VdS 2025 – Electrical cabling systems
- VdS 3145 – Photovoltaic systems
- VdS 6023 – Photovoltaic systems on roofs with flammable building materials
Lightning protection systems and earthing systems
- DIN EN 62305-1 to -4 (IEC 62305-1 to -4)
- Local additional requirements (e.g. state building regulations in Germany)
- DIN 18014
- DIN VDE 0100-540 (IEC 60364-5-54)
Construction regulations
- EN 13501-1/-2, DIN 4102-1/-2 Fire classification of construction products and building elements
- The national and regional construction regulations must be observed with regard to the use of construction products. These include, for example, the state construction regulations in Germany, VKF regulations in Switzerland and OIB directives in Austria