Client references

Hide filters
Building type
Product unit
Building use
Country

From garage to modern office space: A complete infrastructure from floor to ceiling.

For this project, several OBO solutions were combined into one integrated system.

Miniatur Wunderland Hamburg – OBO Bettermann in the warehouse district

Cables had to be installed in the tightest of spaces, while remaining virtually invisible. This is where the cable support systems from OBO Bettermann come into play.

The Mandemaat project in Assen combines architecture with building technology to create a future-proof building

As an ultra-modern, sustainable office building, the Mandemaat project in Assen is considered one of the most sustainable government buildings in the Netherlands. OBO Bettermann enhanced the structure with its products, including from the area of cable support systems.

Robust cable infrastructure for a next-generation data centre

OBO provided the entire cable infrastructure for the AMS4 data centre in Diemen Proven products created a solid foundation for the data centre, where the focus is on reliability and continuity.

Renovation of a conference room in the heart of Kyiv

Event spaces, in particular, rely on offering different power supply options. OBO Bettermann provides a design-oriented solution, along with practical products.

New ETZ Elisabeth Hospital building in Tilburg

A large-scale new building is being constructed for Elisabeth-TweeSteden Hospital (ETZ) in Tilburg, the Netherlands, as an extension to the existing hospital complex.

OBO Cassette Solutions

OBO cassette solutions and Terrazzo floors – the perfect combination for event locations

The OBO cassette solutions offer event locations with different power supply requirements concealed technology for maximum design freedom.

Sprengel Museum Hannover

Sprengel Museum Hanover: Design meets technology – OBO solutions in action

With specially developed Terrazzo lined bodies, OBO enables direct, jointless installation of height-adjustable cassettes in polished screed and Terrazzo floors.

Gottfried Wilhelm Leibniz Library

Gottfried Wilhelm Leibniz Bibliothek, Lower Saxony state library

As the state library of Lower Saxony, Gottfried Wilhelm Leibniz Bibliothek offers not only a growing digital service offering, but many other services as well. The library is important as it provides free access to academic information for all.

The iconic “Twister” megadisco

Twister Dance celebrates a comeback – a party atmosphere with OBO Bettermann

After the fire in November 2023, which completely destroyed the old building, “Twister 2.0” was built. OBO Bettermann delivered cable trays and insulation systems for fast, reliable mounting.