Sporting and event locations
When thousands of people come together, OBO leaves nothing to chance
Whether a sports stadium, events hall or a congress centre – large numbers of people come together in all of these locations and nothing can be left to chance. A safe electrical infrastructure is the basis for successful events. Through robust cable support systems, fire protection systems and solutions for lightning and surge protection, OBO can guarantee safety whenever it is required. Even in exceptional circumstances, a reliable, vandalism-proof supply of power and data is guaranteed.

Our solutions for sporting and event locations:
- Cable trays in a hot-dip galvanised version: The zinc layer thicknesses of these cable trays allow an installation in outdoor and indoor areas with increased corrosion protection requirements. Despite the high humidity and chlorine levels in the air, the zinc coating ensures a long lifespan over multiple decades.
- Deskboxes for power, data and multimedia: In the press centres of sports areas, power, multimedia connections and data transmission via cable are required directly at the workplace of the journalists, in order to guarantee immediate, secure information processing. The OBO Deskbox , which is clamp-fastened to the tabletop, offers all the necessary connection types and can be placed flexibly, meaning that there is always a sufficiently large workspace on the table.
- Cable trays for outdoor areas: In open stadia and arenas, cable trays and support systems must be able to withstand weather conditions for long periods of time without corrosion damage. To achieve this, components with zinc coating thicknesses according to DIN EN ISO 1461 with approx. 40–60 μm are used, such as the OBO cable trays. These have already been installed in countless stadia around the world. For example, in the Philips Stadium in the Dutch city of Eindhoven, where they provide the reliable supply of the LED lighting above the main stand.
Good to know: OBO cable trays can be coated in various RAL shades. This means that not only the visual requirements can be fulfilled, but also increased corrosion protection achieved.
Product highlights for sporting and event locations

PYROLINE® Con D BSK I90/E30 fire protection duct

2-component fire protection foam PYROSIT® NG

Strain relief on three sides, empty housing, internal height 175 mm

Combination arrester V50, 3-pole + NPE with FS 280 V

Vertical ladder, SLM50

Heavy-duty vertical cable ladder SLM 50, 3 m C40

Cable tray MKS 60 FT

US 7 support FT

Wall and support bracket AW 30 FT

Deskbox DBK, 3 sockets, 2x RJ45 Cat. 6

isCon® conductor Professional plus, grey

PYROPLUG® MagicBox, four-sided, interior height 60 mm

Philips Stadium Eindhoven
OBO delivered RKSM cable trays for the LED lightning, that is mounted above the grandstand.

Bettermann AG takes to the ice at the Swiss Life Arena in Zurich
OBO products can be found throughout the entire building complex. A key point was the requirement for seismic design for cable routing using cable support systems.

Museo della Pietà, Milan
In the Museo della Pietà in Milan, OKA trunking from OBO provide a discreet and flexible power supply around Michelangelo's last masterpiece.
LDLC multipurpose hall, near Lyon, sets new standards
The LDLC Arena, located close to the French city of Lyon, is a multipurpose hall, which is privately financed and has been created next to the football stadium of football club Olympique Lyonnais. In future, the RKS-Magic® cable trays and the GR-Magic® mesh cable trays will ensure the safe routing of power and data.
Downloads
Solutions for commercial and residential buildings
Fire protection in electrical technology – a guide to fireproof building installations
Lightning protection guide
Cable support system MKS SKS
Guide to cable support systems
You might also find this interesting

Education buildings
To equip education buildings with electrical technology for the future, individual technologies must be combined with centrally controlled systems. OBO offers the matching solutions for this.

Office and administrative buildings
The world of work is changing continuously, as shown by open space offices. The OBO portfolio contains solutions for the electrical infrastructure that are discreet, flexible and reliable.

Listed buildings
The monument protection is frequently at odds with the requirements for fire protection and lightning protection in buildings. Special solutions need to be found and OBO is happy to take on the challenge.

Shopping centres
Function and design, quality and long life: These are factors that are at the forefront of electrical installations in shopping centres. All these attributes combine the OBO solutions for this area.

Healthcare
In hospitals, care homes and geriatric facilities, solutions from OBO secure a fault-free supply of power and data. They fulfil not only functional but also hygienic criteria.

Hotels and restaurants
Hotels, restaurants or congress centres – many people come together here, so that not only functional but also aesthetic requirements must be fulfilled. This is a challenge that’s tailor-made for OBO.

Logistics buildings
Logistics buildings are characterised by expansive steel and concrete structures. To bridge large support spacings, OBO wide span cable support systems and heavy-duty vertical ladders are the ideal solution.

The construction of living accommodation
There is scarcely another place in which we feel as safe as within our own four walls. OBO offers a variety of electrical components for a safe and comfortable life.

OBO solutions for commercial and housing construction
With many years of expertise and a comprehensive portfolio, we can ensure safe electrical installations in any building – from homes, to offices, all the way to hospitals and sports stadiums.