Office and administrative buildings
Efficient electrical infrastructure for office buildings
The modern working world is constantly changing. This is shown particularly by the increasingly popular open space offices, which are characterised, for example, by floor to ceiling windows and large office spaces without partitions. The key here is to use the available space to the maximum and be as flexible as possible with regard to furnishings. The electrical infrastructure and the routing of the cables for power and data must adapt to these requirements. One of the simplest exercises for the OBO portfolio.

OBO solutions for modern office buildings:
- OKA open, screed-flush trunking system: With the OKA floor-flush trunking system, large volumes can be routed in the floor. The trunking can be opened and closed using lockable covers and the floor boxes can be moved within the course of the trunking. This allows the flexible adaptation of outlets for current and data to changes in the room furnishings.
- GES service outlets: Service outlets supply workstations and other points in the middle of the room with power and data connections via the floor. Ideal for modern office design. The service outlets are available in round and rectangular designs. The variants Metal and plastic and metal variants blend discreetly into the individual room design.
- Deskboxes: The OBO Deskboxes offer direct access to power, data and multimedia connections for every workplace. Three different Deskbox solutions in high-quality materials and elegant designs are available to meet individual requirements: The freely placeable Deskbox DB , the lowerable Deskbox DBV and the foldable DBK Deskbox .
- Rapid 80 double trunking: The Rapid 80 double trunking unifies design and function in one system in an uncomplicated and convincing manner. The two fully separate trunking compartments are used to accept cables with different potentials, for example data and heavy current cables. This excludes electromagnetic interference in the parallel cable run.
- Rapid 80 with integrated windowsill: The Rapid 80 can be fastened to the wall using a panel and its depth can also be adjusted. Firstly, slats are snapped onto the panels, forming a flush closure as a windowsill.
- Black-coated cable trays: What connects modern office buildings and office landscapes in historic old buildings? Both place great emphasis on an impressive appearance. Frequently, open ceilings can be found in these building types. The OBO cable trays with a black, powder-coated finish are ideal for use in environments such as these, which have aesthetic requirements.
Product highlights for office and administrative buildings

Installation duct with PYROLINE® Rapid PLM fire protection mesh, duct height 80 mm, FS

2-component fire protection foam PYROSIT® NG

Combination arrester V50, 3-pole + NPE with FS 280 V

Device installation trunking Rapid 80, trunking width 170, trunking height 70, symmetrical

Deskbox DBK, 3 sockets, 2x RJ45 Cat. 6

Surge protection module 230 V

Service pole, type ISS140110

Trunking unit, blank, height 60−110 mm

GES6 service outlet with locking slider

Installation duct with PYROLINE® Rapid PLM fire protection mesh, duct height 80 mm, pure white

Surge arrester V20, 3-pole + NPE and remote signalling, 280 V

Service pole, type ISSRHSM45

New Axel Springer Building
A symbol of changing media and collaboration: a cubic building awash with light is being built right next to the adjacent high-rises and the Axel Springer Passage in Berlin.

New head office of BNP Paribas Fortis in Brussels
In this project, OBO underfloor systems were used in a very special manner: The cover of the GES9M-2 service outlets were used as access points for the testing and maintenance of underfloor smoke detectors.

Mobile working made easy – the HoverCube from OBO makes everything flexible
Thanks to the HoverCubes from OBO, no one needs to worry about power supply for laptops, mobile devices and tablets.

Stylish Porsche Studio in Singapore relies on OBO Bettermann
OBO Bettermann supports this unique project through the flexibility offered by the appropriate UDHOME4 floor boxes.

Antwerp Town Hall
Antwerp Town Hall was completely restored between 2018 and 2022. Part of the work: Underfloor systems from OBO. The town hall in Antwerp is listed as a UNESCO World Heritage Site.
Downloads
You might also find this interesting

Education buildings
To equip education buildings with electrical technology for the future, individual technologies must be combined with centrally controlled systems. OBO offers the matching solutions for this.

Listed buildings
The monument protection is frequently at odds with the requirements for fire protection and lightning protection in buildings. Special solutions need to be found and OBO is happy to take on the challenge.

Shopping centres
Function and design, quality and long life: These are factors that are at the forefront of electrical installations in shopping centres. All these attributes combine the OBO solutions for this area.

Healthcare
In hospitals, care homes and geriatric facilities, solutions from OBO secure a fault-free supply of power and data. They fulfil not only functional but also hygienic criteria.

Hotels and restaurants
Hotels, restaurants or congress centres – many people come together here, so that not only functional but also aesthetic requirements must be fulfilled. This is a challenge that’s tailor-made for OBO.

Logistics buildings
Logistics buildings are characterised by expansive steel and concrete structures. To bridge large support spacings, OBO wide span cable support systems and heavy-duty vertical ladders are the ideal solution.

Sporting and event locations
When thousands of people converge, nothing must be left to chance. This also applies to building infrastructure. OBO supplies reliable products, thus guaranteeing safety.

The construction of living accommodation
There is scarcely another place in which we feel as safe as within our own four walls. OBO offers a variety of electrical components for a safe and comfortable life.

OBO solutions for commercial and housing construction
With many years of expertise and a comprehensive portfolio, we can ensure safe electrical installations in any building – from homes, to offices, all the way to hospitals and sports stadiums.