Library

Education buildings

Individual technology meets centrally controlled systems

The requirements for the equipment of modern education buildings are increasing continuously and must be taken into account both for new buildings and during renovations. The challenge: Individual technical equipment must be harmonised with centrally controlled systems. Here, ingenious cable management systems or modern media poles offer the solution, in order to meet the requirements of modern education facilities.

As schools and other educational facilities are some of the building types frequented by a large number of people on a regular basis, fire protection measures are expressly required. These are intended to protect the building and the people inside.

Gottfried Wilhelm Leibniz Library

OBO BlackLine – stylish electrical installations in black

Elegant design meets proven quality: Discover the BlackLine products for modern commercial and residential construction.

OBO equips education buildings with a future-proof and safe electrical installation:

  • Metal ducts for device installation: Their robust design means that the OBO sheet steel or aluminium device installation ducts are ideally suited for use in schools, universities and research facilities. Here, large volumes of cables and also larger cable cross-sections must frequently be routed, for example to operate different kinds of measurement, inspection and testing systems. With their dimensions of up to 210 mm x 90 mm, OBO sheet steel and aluminium ducts offer sufficient space for device installation and cable routing. Their powder-coated surface makes them particularly resistant. The special triangular shape of the OBO desk ducts means that they are ideal for installation on or above laboratory benches. Here and here , you will find different variants.
  • Halogen-free cable ducts: For safe cable routing in public areas, OBO offers halogen-free ducts for device installation and cable routing. The plastic ducts effectively reduce the fire load and are safe choice, particularly in educational facilities. In case of fire, they reduce the proportion of toxic smoke gases and do not develop any corrosive substances.
  • The OBO media pole for schools: The OBO media poles were developed specially for schools.  With their modular structure and their numerous configuration options, they offer the ideal basis for combining individual equipment options with the simple integration of centrally controlled systems. Everything necessary can be included in the pole, from the securing of electrical systems, individual light control, supplying information from central communication and emergency call systems, through to displaying the time: With the OBO media poles, all the installation requirements for modern learning can be implemented in a single system in a well-thought-out manner. The media poles are available as freely configurable variants or in a total of eight preconfigured variants. The freely configurable variants are characterised by countless selection options, meaning that they can be adapted individually to the requirements of the appropriate classrooms or training rooms. The preconfigured variants are successfully already in use around the world in education buildings. If you choose one of these variants, you can profit from shortened delivery times and even more rapid availability.

Integrated school in Rust

To Project
Media kiosks installed during school renovation

Schiller high school in Offenburg

To Project

Futurium Berlin

To Project

Escape routes

Lightning protection and lightning and surge protection in buildings

You might also find this interesting

Commercial and residential buildings

Office and administrative buildings

The world of work is changing continuously, as shown by open space offices. The OBO portfolio contains solutions for the electrical infrastructure that are discreet, flexible and reliable.

Commercial and residential buildings

Listed buildings

The monument protection is frequently at odds with the requirements for fire protection and lightning protection in buildings. Special solutions need to be found and OBO is happy to take on the challenge.

shopping centre, mall

Commercial and residential buildings

Shopping centres

Function and design, quality and long life: These are factors that are at the forefront of electrical installations in shopping centres. All these attributes combine the OBO solutions for this area.

corridor, doctor's surgery

Commercial and residential buildings

Healthcare

In hospitals, care homes and geriatric facilities, solutions from OBO secure a fault-free supply of power and data. They fulfil not only functional but also hygienic criteria.

Hotel Gallia

Commercial and residential buildings

Hotels and restaurants

Hotels, restaurants or congress centres – many people come together here, so that not only functional but also aesthetic requirements must be fulfilled. This is a challenge that’s tailor-made for OBO.

Warehouse, logistics

Commercial and residential buildings

Logistics buildings

Logistics buildings are characterised by expansive steel and concrete structures. To bridge large support spacings, OBO wide span cable support systems and heavy-duty vertical ladders are the ideal solution.

stadium

Commercial and residential buildings

Sporting and event locations

When thousands of people converge, nothing must be left to chance. This also applies to building infrastructure. OBO supplies reliable products, thus guaranteeing safety.

sofa, living room

Commercial and residential buildings

The construction of living accommodation

There is scarcely another place in which we feel as safe as within our own four walls. OBO offers a variety of electrical components for a safe and comfortable life.

Building, Glass

Construction industry

OBO solutions for commercial and housing construction

With many years of expertise and a comprehensive portfolio, we can ensure safe electrical installations in any building – from homes, to offices, all the way to hospitals and sports stadiums.

Contact

OBO Bettermann Export GmbH & Co. KG

Do you have any questions on this topic? We are glad to help!