Listed buildings
Reliable solutions for historic structures
Listed buildings not only stand out through their impressive appearance, they also have a culturally historic value. This is why they are protected, in order to maintain them for eternity, if possible.
Listed buildings are a real challenge for electrical installations and their renovation is complex. This is because monument protection and the current requirements for fire protection, lightning protection and technical equipment are frequently at odds. This is why special solutions must be found. A fine thing then that special solutions are standard for OBO.

OBO provides safe electrical installations in listed buildings:
- Fire protection ducts In case of fire, escape and rescue routes must always remain free of fire and smoke. This is because they are not only used for safe evacuation, but also represent key points of attack for the fire brigades. OBO fire protection ducts are a secure solution for installation in escape and rescue routes, as they actively encapsulate the fire load, thus preventing a fire spread.
- Underfloor systems: OBO underfloor systems unite the maximum of functionality with high-quality design. An example: The OBO GES9M service outlet – it offers a refined solution for installation in historical wooden floors.
- Cable insulation: With the OBO cable insulation, you are always on the safe side. It is particularly suitable for including previously routed cable bundles in fire protection measures at a later time. Special applications for ceilings in existing buildings are also a part of our portfolio, as are fire protection systems in wooden beamed ceilings. Fire protection and wood this may sound like a contradiction, but it need not be. If electrical installations in wooden buildings have to be run through walls and ceilings with a fire resistance period, then they must be insulated, in order to prevent the spread of fire. This can be done using fire protection insulation, which seals ceiling and wall penetrations reliably against fire and smoke with a soffit of non-combustible material. The OBO insulation systems offer comprehensive protection for the maintenance of fire sections – particularly for wooden components.
Product highlights for listed buildings

Ridge conductor holder with tensioning spring

Installation duct with PYROLINE® Rapid PLM fire protection mesh, duct height 80 mm, FS

PYROLINE® Con D BSK I90/E30 fire protection duct

2-component fire protection foam PYROSIT® NG

PYROCOMB® Intube pipe shell, Ø 120 mm

GES9M-2 service outlet with handle clamp

Height-adjustable cassette with cord outlet, RKSNUZD3, stainless steel

Installation duct with PYROLINE® Rapid PLM fire protection mesh, duct height 80 mm, pure white

Roof conductor holder for tiled roofs, Rd 8−10

Gutter clamp RK-FIX Cu

Round conductor, copper
Downloads
You might also find this interesting

Education buildings
To equip education buildings with electrical technology for the future, individual technologies must be combined with centrally controlled systems. OBO offers the matching solutions for this.

Office and administrative buildings
The world of work is changing continuously, as shown by open space offices. The OBO portfolio contains solutions for the electrical infrastructure that are discreet, flexible and reliable.

Shopping centres
Function and design, quality and long life: These are factors that are at the forefront of electrical installations in shopping centres. All these attributes combine the OBO solutions for this area.

Healthcare
In hospitals, care homes and geriatric facilities, solutions from OBO secure a fault-free supply of power and data. They fulfil not only functional but also hygienic criteria.

Hotels and restaurants
Hotels, restaurants or congress centres – many people come together here, so that not only functional but also aesthetic requirements must be fulfilled. This is a challenge that’s tailor-made for OBO.

Logistics buildings
Logistics buildings are characterised by expansive steel and concrete structures. To bridge large support spacings, OBO wide span cable support systems and heavy-duty vertical ladders are the ideal solution.

Sporting and event locations
When thousands of people converge, nothing must be left to chance. This also applies to building infrastructure. OBO supplies reliable products, thus guaranteeing safety.

The construction of living accommodation
There is scarcely another place in which we feel as safe as within our own four walls. OBO offers a variety of electrical components for a safe and comfortable life.

OBO solutions for commercial and housing construction
With many years of expertise and a comprehensive portfolio, we can ensure safe electrical installations in any building – from homes, to offices, all the way to hospitals and sports stadiums.