hospital, corridor

Electrical infrastructure for healthcare

Best-possible supply guaranteed

The healthcare sector places particular requirements on electrical installations: Here, not only functional but also hygienic standards must be complied with. In addition, a reliable supply of the medical devices with power and data is essential, in order to allow the best-possible supply of the patients.

OBO solutions secure a high-performance electrical infrastructure in doctors’ surgeries and hospitals, and in care homes and assisted living. In this way, we help healthcare facilities to improve the efficiency of their processes, meaning that both patients and medical personnel can receive the optimum technical support.

corridor, doctor's surgery

OBO solutions for healthcare:

  • Magic® cable trays: Large volumes of cables run for kilometres through the multi-layered building complexes of hospitals. Of key importance is the sufficient ventilation of the power and data cables. This is not a problem for the Magic® cable trays, whose tray bases are more than 30% perforated. The high amount of holes means that they can also be used beneath sprinkler systems. Installed above fire protection ceilings, the Magic® trays, which are suitable for the maintenance of electrical function, make a major contribution to the securing of escape and rescue routes in case of fire.
  • Antibacterial sheet steel and aluminium trunking: OBO sheet steel and aluminium trunking can be coated with a special power coating, which has an antibacterial action, even against tough germs. They are suitable for use in doctors’ surgeries, hospitals or care facilities, where they can help to reduce the risk of infection.
  • Cable systems approved for the maintenance of electrical function: Together with the special cables for the maintenance of electrical function, the Magic® cable tray system forms cable systems tested and approved for the maintenance of electrical function in case of fire. This means that key systems, such as escape route lighting, alarm and signal systems or fire brigade lifts, can continue to function for up to 90 minutes, even if there is a fire. Essential minutes for the safe evacuation of injured people from the building!
  • Lightning and surge protection: According to the lightning protection risk analysis, hospitals are evaluated as having the highest protection requirements. This protection is offered by the OBO lightning and surge protection systems, whose interactions are coordinated perfectly. These include air-termination and conductor systems, equipotential bonding systems, earthing systems and integrated lightning and surge protection.
Enjoy Gym Fitness Center in Oviedo

OKB system seamlessly provides treadmills with power and data

To Project
AZ Delta Clinic, Belgium

AZ Delta hospital, Belgium

To Project

Escape routes

Lightning protection and lightning and surge protection in buildings

You might also find this interesting

Gottfried Wilhelm Leibniz Library

Commercial and residential buildings

Education buildings

To equip education buildings with electrical technology for the future, individual technologies must be combined with centrally controlled systems. OBO offers the matching solutions for this.

Commercial and residential buildings

Office and administrative buildings

The world of work is changing continuously, as shown by open space offices. The OBO portfolio contains solutions for the electrical infrastructure that are discreet, flexible and reliable.

Commercial and residential buildings

Listed buildings

The monument protection is frequently at odds with the requirements for fire protection and lightning protection in buildings. Special solutions need to be found and OBO is happy to take on the challenge.

shopping centre, mall

Commercial and residential buildings

Shopping centres

Function and design, quality and long life: These are factors that are at the forefront of electrical installations in shopping centres. All these attributes combine the OBO solutions for this area.

Hotel Gallia

Commercial and residential buildings

Hotels and restaurants

Hotels, restaurants or congress centres – many people come together here, so that not only functional but also aesthetic requirements must be fulfilled. This is a challenge that’s tailor-made for OBO.

Warehouse, logistics

Commercial and residential buildings

Logistics buildings

Logistics buildings are characterised by expansive steel and concrete structures. To bridge large support spacings, OBO wide span cable support systems and heavy-duty vertical ladders are the ideal solution.

stadium

Commercial and residential buildings

Sporting and event locations

When thousands of people converge, nothing must be left to chance. This also applies to building infrastructure. OBO supplies reliable products, thus guaranteeing safety.

sofa, living room

Commercial and residential buildings

The construction of living accommodation

There is scarcely another place in which we feel as safe as within our own four walls. OBO offers a variety of electrical components for a safe and comfortable life.

Building, Glass

Construction industry

OBO solutions for commercial and housing construction

With many years of expertise and a comprehensive portfolio, we can ensure safe electrical installations in any building – from homes, to offices, all the way to hospitals and sports stadiums.

Contact

OBO Bettermann Export GmbH & Co. KG

Do you have any questions on this topic? We are glad to help!