Logistics buildings
Robust solutions for rough environments
Industrial plants and logistics buildings require effective cable routing, which must also be robust, in order to withstand the rough environment. The electrical supply of logistics areas frequently comes from concrete supports, walls, with clamp fastenings on steel girders or on concrete roof ties under the hall roof. This guarantees sufficient freedom of movement on the floor. Here, it is important to bridge large support spacings. A challenge for which the wide span cable support systems and heavy-duty vertical ladders from OBO are predestined.

OBO solutions for logistics buildings:
- Wide span cable trays and ladders: With the cable trays and cable ladders from the OBO wide span system, cables can be routed with ease over long distances with a support spacing of up to 8 m.
- Vertical ladders for high cable loads: For decades, the robust OBO cable support systems, which have been tested for the different areas of application, have been used successfully in the field of electrical installations. They have also proven their worth time and again in industrial environments and in logistics buildings. All the challenges of electrical installations can be mastered professionally and safely with OBO vertical ladders.
- Stand and ceiling fastening: A solid stand for floor fastening ensures secure mounting on the floor. A solid ceiling fastening at the top can easily be adjusted to different heights.
- Service poles for industrial applications: The OBO service poles for industrial applications combine power, data and compressed air connections in a compact and robust manner. Changes of location, for example in the adaptation of production processes, can be implemented particularly quickly and simply. The ISS base profile is fully compatible with the item MB Building Kit System known in machine and system construction.
- Hovercube: With the space-saving HoverCubes of types VH and VHF from OBO, annoying extension cables and hoses to supply workplaces in the production and logistics are a thing of the past. The compact suspended distributors can be suspended from the ceiling and thus freely positioned in the room. They offer safe, logical working at the workstation.
Product highlights for logistics buildings

Vertical ladder, SLM50

Service pole, type ISS140110

PYROPLUG® MagicBox, four-sided, interior height 60 mm

Bus connector for PDP-OS

Power supply for PDP-OS, 5 V

Connectable data cable protection, 2-pole, indirect earthing, 5 V

Wide span cable ladder WKLG 110 FS

Wide span cable tray WKSG 110 FS

Trunking, type WDK 60090

Cable duct, type LKM 60100

HoverCube VH-4, with FI/LS, 2x protective contact sockets

VGP Park Brasov
In the future, the cable support systems from OBO Bettermann will ensure that cables, and thus data, can be routed securely from A to B.
Downloads
Solutions for commercial and residential buildings
Fire protection in electrical technology – a guide to fireproof building installations
Lightning protection guide
Guide to cable support systems
Welded cable ladder system
Service poles for industrial applications
You might also find this interesting

Education buildings
To equip education buildings with electrical technology for the future, individual technologies must be combined with centrally controlled systems. OBO offers the matching solutions for this.

Office and administrative buildings
The world of work is changing continuously, as shown by open space offices. The OBO portfolio contains solutions for the electrical infrastructure that are discreet, flexible and reliable.

Listed buildings
The monument protection is frequently at odds with the requirements for fire protection and lightning protection in buildings. Special solutions need to be found and OBO is happy to take on the challenge.

Shopping centres
Function and design, quality and long life: These are factors that are at the forefront of electrical installations in shopping centres. All these attributes combine the OBO solutions for this area.

Healthcare
In hospitals, care homes and geriatric facilities, solutions from OBO secure a fault-free supply of power and data. They fulfil not only functional but also hygienic criteria.

Hotels and restaurants
Hotels, restaurants or congress centres – many people come together here, so that not only functional but also aesthetic requirements must be fulfilled. This is a challenge that’s tailor-made for OBO.

Sporting and event locations
When thousands of people converge, nothing must be left to chance. This also applies to building infrastructure. OBO supplies reliable products, thus guaranteeing safety.

The construction of living accommodation
There is scarcely another place in which we feel as safe as within our own four walls. OBO offers a variety of electrical components for a safe and comfortable life.

OBO solutions for commercial and housing construction
With many years of expertise and a comprehensive portfolio, we can ensure safe electrical installations in any building – from homes, to offices, all the way to hospitals and sports stadiums.