Solutions for wind turbine nacelles
The nacelle is located in the tower of the wind power plant. The two components are connected via a rotating joint. The rotor, consisting of the hub and individual rotor blades, is located at the front of the nacelle. The nacelle transfers the loads resulting from the rotor and all installed components to the foundation via the tower.
The wind turbine nacelle is often referred to as the powerhouse, as it is the core of the wind turbine. Some of the most important components of the plant are inside, such as the generator for producing electricity. However, the highest vibrations and oscillations occur in the area of the nacelle and the tower head. This means that the installation systems installed there are also subject to special requirements. OBO offers the maximum safety in this area with protection solutions for the wind turbine nacelle.

OBO system solutions for wind turbine nacelles
- Surge arrester V20 with a total discharge capacity of 60 kA (20/40 kA/pole)
- Surge protection for high-speed networks up to 1 GB with data line protection devices for high-speed networks up to 1 GB
- GR-Magic® mesh cable tray with the patented, plug-in connection system
- Wall and support bracket for screwless mesh cable tray fastening
- Robust junction boxes for safe IP protection of electrical cabling
- Magnetic card and holder for recording pulsed and lightning currents
- Insulated air-termination rod for inner-routed isCon conductors with side exit: explaining the isCon system
Product highlights for the nacelles of wind turbines

Surge arrester V20, 3-pole + NPE and remote signalling, 280 V

Surge protection for high-speed networks up to 10 GBit (Class EA/CAT6A)

Mesh cable tray GR-Magic® 55 FT

Junction box T60, with knock-out entries and 3 x V-TEC VM20 + locknuts

Magnetic card and holder MK-B

Wall and support bracket AWG 15 FT

isCon® conductor, Professional plus black
Downloads for the nacelle of wind turbines
You might also find this interesting

Earthing solutions for wind power plants
The comprehensive protection of the electrical installations in wind power plants starts at the very bottom, with the foundations. OBO offers various solutions in the field of earthing systems especially for the foundations of wind power plants.

Protection solutions for the tower of wind power plants
The tower of a wind power plant requires a particularly stable and robust electrical infrastructure. The cable ladder and vertical cable ladder systems from OBO meet this challenge easily.

Protection solutions for the basic of wind power plants
Between the foundation and the actual tower is the base of the wind power plant. With the protection solutions from OBO, the electrical devices installed in the base of wind turbines are fully protected against surge damage:

OBO solutions for wind power plants
We are part of the energy revolution and offer a complete solution for the electrical equipment of wind power plants − from the foundation to the nacelle.