Protection solutions for the foundation of wind power plants
Between the foundation and the actual tower is the tower base or the base of the wind power plant. The tower and foundation are connected via the foundation component. For this, both a single or double flange as well as the quiver or basket system can be used.
The tower base often also houses the control cabinets as well as the surge protective devices of the plant. Surge protection systems for wind power plants are of fundamental importance, as the plants are particularly susceptible to direct lightning strikes due to their height, shape and size. The plants contain many electronic devices that can be damaged by surges. But not only the individual electronic components can be damaged, there is also the risk of a complete failure of the power plant, resulting in repair costs and loss of revenue.
Wind power plants are often located in an elevated position. This is where their degree of utilisation is the highest, but there is also the risk of damage due to lightning strikes and surges. An additional danger to the power plant is discharges caused by air currents from the rotating parts of the wind turbine. To ensure safe and reliable operation of the wind power plant, appropriate surge protection is therefore essential. For this, all metallic structures, metallic installations, internal systems as well as externally conductive parts and services entering the wind power plant must be connected directly or indirectly to the equipotential bonding via the lightning current and surge arrester. In this way, complete lightning protection equipotential bonding is achieved.

Our products for a protected wind turbine base
- Lightning current arrester MCF-35 for reliable lightning current equipotential bonding
- The plug-in, universal data line protection PDP, combining lightning and surge protection
- The RKS-Magic® plug-in cable trays, representing the three fundamental aspects of efficiency, safety and stability.
- The Quick-Pipe system, offering a clever system and a reliable fastening solution with the Quick clamps, Quick-Pipe electrical installation pipes and the associated fittings.
- The BigBar equipotential busbar, suitable for both lightning protection equipotential bonding and normal equipotential bonding.
Product highlights for the base of wind turbines
Downloads for the base of wind power plants
You might also find this interesting

Earthing solutions for wind power plants
The comprehensive protection of the electrical installations in wind power plants starts at the very bottom, with the foundations. OBO offers various solutions in the field of earthing systems especially for the foundations of wind power plants.

Protection solutions for the tower of wind power plants
The tower of a wind power plant requires a particularly stable and robust electrical infrastructure. The cable ladder and vertical cable ladder systems from OBO meet this challenge easily.

Solutions for wind turbine nacelles
The core of any wind turbine is the nacelle. OBO offers the maximum safety in this area with protection solutions such as surge protection or interception and arrester systems.

OBO solutions for wind power plants
We are part of the energy revolution and offer a complete solution for the electrical equipment of wind power plants − from the foundation to the nacelle.