Telekom Flagship Store Hamburg

Telekom flagship store in Hamburg

With the new Telekom flagship store in Hamburg, LEPEL & LEPEL is setting a strong signal for sustainable retail design.

Telekom flagship store in Hamburg

Function meets design meets sustainability

The interior design and planning team from Cologne-based LEPEL & LEPEL brought the Hamburg location back to life in a way never seen before as part of the retail design for Telekom rolled out across Germany – transforming customers into fans and bringing an entirely new concept to shop retail.

Telekom Flagship Store Hamburg
Telekom Flagship Store Hamburg
Telekom Flagship Store Hamburg
Telekom Flagship Store Hamburg

Located centrally in Hamburg, the sustainable flagship store invites customers to linger, impressing with select materials and a design that reflects the Hanseatic City. The project is called “Waterkant” (waterfront), which can also be seen on the container walls.

Europe’s largest shop was presented on 875 square metres, revolving around the topic of water.

As a constant throughout the Telekom retail design, the “clear hull” conceptualised by LEPEL & LEPEL provides a frame for the entire interior with black ceilings and walls, making the magenta branding shine. One highlight is the magenta staircase connecting the two storeys.

With a new shop design, Telekom is focusing on sustainability and environmental awareness. The company uses sustainable raw materials, recycled furniture and furniture produced by local manufacturers. Lavish greenery on the ceiling enhances the ambience.

Cable trays  from OBO securely route cables under the ceiling. OBO BlackLine offers the right symbiosis of design and function in this stylish setting.

Uncomplicated installation ensures smooth collaboration between trades and the fast realisation of projects.

The product range also excels in the areas of sustainability and environmental compatibility.  Because all OBO BlackLine products are flexible, durable and characterised by high-quality materials and surfaces. When it comes to building repurposing, they are ideally suited to being dismantled and reinstalled for the next application.

Circular products such as those of the OBO BlackLine range make a crucial contribution to increased sustainability in construction. The black Cable trays could not have been used more effectively in this project.

Telekom Flagship Store Hamburg

Project information

  • Product categories
  • ArchitectLEPEL & LEPEL
  • Location and countryHamburg - Germany
  • Building size835 m²
  • PhotographyHGEsch Photography

OBO BlackLine – Stilvolle Elektroinstallation in Schwarz

Elegantes Design trifft auf bewährte Qualität: Entdecken Sie die BlackLine-Produkte für moderne Gewerbe- und Wohnräume.