Cable support systems

Design and functional features of cable support systems

Cable support systems are essential components of a safe and efficient electrical installation. They are used not only for tidy cable routing and fastening, but also have to withstand a wide range of mechanical and environmental loads. The selection of the correct system is dependent on various factors, such as material, corrosion resistance and operating environment. We will explain the most important design and functional properties of cable support systems – from the materials used, to surface coatings through to corrosion protection measures.

FAQ – cable support system basics

What is a cable support system?

Where are cable support systems installed?

What materials are cable support systems made of?

What components does a cable support system have?

What different cable support systems are there?

What are fittings for?

What are support elements?

What are mounting elements used for?

What accessory parts are available?

What is the support distance?

Are external fastening elements part of the cable support system?

Corrosion and corrosion protection

Generally, a distinction is made between the following corrosion mechanisms:

 

Surface corrosion

  • Unprotected, unalloyed steel oxidises extensively due to moisture and oxygen
  • Classic rust formation on steel
  • If the rust formation location is limited, then this is termed hole or sink corrosion
Surface corrosion

Contact or bi-metallic corrosion

  • Caused by the different electrochemical potentials of two metals (e.g. zinc and VA)
  • Difference between precious metals and base metals
    • Precious metals: electrochemical potential > 0
    • Base metals: electrochemical potential < 0
  • The baser partner oxidises 
  • Observe the area rule:
    • Good ratio: base large, precious small
    • Poor ratio: precious large, base small
Bimetal

 

 

Gap corrosion

  • This affects unalloyed steel and stainless steel (this also applies if the gap is caused by plastic on steel)
  • Caused by moisture in narrow gaps (< 1 mm)
  • The electrolyte in the gap “acidifies” (i.e. the pH value falls), the electrolyte on the outside becomes alkaline (i.e. the pH value increases)
  • Reaction products form, which can finally be seen as rust, hollowing out the gap
gap


 

Hole corrosion on stainless steels

  • Passive layer of the stainless steels is harmed, due primarily to chloride
  • Local spot corrosion can form, which hollows out the steel at the appropriate point
  • In addition, tension crack corrosion can occur if there are tensions in the material (material cracks along the grain borders)
Pitting corrosion

 

Corrosion of galvanisations

  • Zinc uses carbon from the air to form a protective zinc carbonate covering layer after a few days
  • If the zinc surface is exposed to moisture, then white rust will form before the covering layer can form
  • Zinc is particularly prone to corrosion if salts exist (usually chloride, sulphate). This causes the zinc to be removed very quickly, meaning that the steel is unprotected
White rust

Electrochemical series of the metals

                     

small/largeZn (FS and FT)AICuVACuZn
Zn (FS and FT)
  •  
  •  
xx
  •  
AI
  •  
  •  
xx
  •  
Cu
  •  
  •  
  •  
  •  
  •  
VA
  •  
  •  
  •  
  •  
  •  
CuZn
  •  
  •  
  •  
  •  
  •  
  • Moderate to no corrosion
  • Moderate corrosion

   x  Heavy corrosion

 

The precondition for corrosion is a conductive medium that connects the metal combination. The more damp and contaminated the atmosphere is, the more pronounced the contact corrosion.

Surfaces

G

FS

FT/(DD)

Electrogalvanised

Hot galvanised

Hot-dip galvanised/(Double Dip)

 

Materials

A2

A4

A5

Stainless steel

Stainless steel

Stainless steel

Special solutions (on request)

FTSO

FSK/FTK

Special layer thickness

Plastic coating

Surfaces

The following galvanisation surfaces can be applied to improve corrosion protection:

Galvanisation

  • Application of the zinc covering using an electrolysis method (direct current)
  • Normal layer thicknesses, approx. 5–15 μm
  • Retreatment normally in the form of passivation and/or sealing

Standards: DIN EN ISO 19598 & DIN EN ISO 4042 
Applications: Indoor areas without harmful substances, e.g. offices, sales rooms – corrosivity category according to DIN EN ISO 12944-2: C1
Examples: Mesh cable trays and connection elements

 

Electrogalvanizing

Strip galvanisation

  • During the strip galvanisation process, also termed sendzimir galvanisation, the steel strip is galvanised in a continuous process
  • Materials: DX51D
  • Normal layer thicknesses (Z 275) approx. 13–27 μm
  • Retreatment of the coil possible in the form of passivation and/or sealing

Standards: DIN EN 10346
Applications: Indoor areas in which condensation can occur, e.g. sports halls or warehouses – corrosivity category according to DIN EN ISO 12944-2: Up to C2
Examples: Cable trays, covers

Strip galvanizing

Hot-dip galvanisation

  • The fully formed product is coated using a dipping method
  • Materials: C9D, DC01, DD11, S235JR
  • Normal layer thicknesses, approx. 45–85 μm

Standards: DIN EN ISO 1461
Applications: Indoor areas with a certain level of moisture and impurity, outdoor areas with medium levels of contamination, e.g. laundries, urban atmosphere – corrosivity category according to DIN EN ISO 12944-2: To C3 (depending on layer thickness, up to C4)
Examples: Cable ladders, mesh cable trays, suspended supports and brackets

hot-dip galvanizing

 

Hot-dip coating (Double Dip)

  • Zinc-aluminium coating according to DIN EN 10346
  • The material to be galvanised then passes through two baths: The first contains pure zinc, the second a zinc-aluminium alloy

Standards: DIN EN 10346

Hot-dip coating

 

Zinc slat coating 

  • Processing of untreated steel to small parts, such as screws or washers 
  • Subsequent coating in the immersion spinning method, with an anorganic, zinc and aluminium-rich substance 
  • Layer thickness: 5–20 µm 
  • Cathodic corrosion protection allows small scratches, e.g. due to transport or mounting 

Standards: DIN EN 13858, DIN EN ISO 10683 
Applications: Interior, exterior
Examples: Connection elements, fastening elements

Zinc flake coating

Plastic coating

  • Plastic coating through electrostatically charged plastic powder
  • Coating for reasons of corrosion protection or for decorative reasons
  • Particularly good adhesion through pretreatment of the components with different fluids
  • Plastic powder made of epoxy and/or polyester resins, as well as polyurethane
  • Normal layer thicknesses, approx. 70–100 μm
  • Coating of various system components possible with the following surfaces:
    • Strip galvanised (FS) and hot-dip galvanised (FT)
    • Electrogalvanised (G) and aluminium (Al)
Plastic coating

Standards: DIN 55633/55634

Corrosion protection applications:

  • Hot-dip galvanised system components with coating (Duplex)
  • Very resistant to moisture, impurities and chemical influences
  • Buildings with continuous condensate formation and strong impurities
  • Corrosivity category according to DIN EN ISO 12944-2: Up to C5

Decorative reasons:

  • Special visual requirements, appropriate to the colour design of the structure
  • Coloured separation or assignment of different functions
  • Available in all RAL colours

Materials

Stainless/rustproof steel

 

  • The entry of oxygen causes a chromium oxide layer to form (passive layer), which protects against corrosion 
  • If the passive layer is damaged, e.g. by cutting, it forms again through further entry of oxygen 
Materials
  • Materials according to the alloy composition:
    • A2: 
      • 1.4301 (AISI 304) 
      • 1.4303 (AISI 305/308) 
      • 1.4310 (AISI 301) 
      • 1.4567 (AISI 304Cu)
    • A4: 
      • 1.4401 (AISI 316) 
      • 1.4404 (AISI 316L) 
      • 1.4435 (AISI 316L) 
      • 1.4571 (AISI 316Ti) 
      • 1.4578 
    • A5: 
      • 1.4529 
      • 1.4547 
      • 1.4462 
  • Standard: EN 10088

 

  • Corrosivity category according to DIN EN ISO 12944-2: 
    • A2: to C3 
    • A4: to C5 
    • A5: to CX
  • Overview of key alloy elements
ElementProperties in the steel
Nickel
  • Stabilises the structure (austenite former) 
  • Increases stability and toughness 
  • Increases the resistance to tension crack corrosion
Molybdenum
  • Increases the pitting resistance 
  • Increases the resistance to tension crack corrosion
Titanium
  • Stabilises the structure (carbide former) 
  • Increases resistance to intercrystalline corrosion
Nitrogen
  • Stabilises the structure (austenite former) 
  • Increases stability

 

Corrosivity categories according to DIN EN ISO 12944-2:2018

 

Corrosivity category

Mass loss/thickness reduction relative to the area (after the first year of warehouse removal)

Example of typical environments (only for information purposes)

 

Unalloyed steel

Zinc

Open air

Interior

 Mass loss g/m²Thickness reduction µmMass loss g/m²Thickness reduction µm  
C1
negligible
≤ 10≤ 1.3≤ 0.7≤ 0.1–Heated building with neutral atmosphere, e.g. offices, sales areas, schools, hotels
C2
low
> 10 to 200> 1.3 to 25> 0.7 to 5> 0.1 to 0.7Atmosphere with low degree of impurity: Usually rural areasUnheated buildings, in which condensation can occur, e.g. warehouses, sports halls
C3
medium
> 200 to 400> 25 to 50> 5 to 15> 0.7 to 2.1Urban and industrial atmosphere with medium sulphur dioxide load; and coastal atmosphere with low salt loadProduction rooms with high humidity and a certain amount of air impurities, e.g. food processing plants, laundries, breweries, dairies
C4
heavy
> 400 to 650> 50 to 80> 15 to 30> 2.1 to 4.2Industrial atmosphere and coastal atmosphere with medium salt loadChemical plants, shipyards near the coast and harbours
C5
very heavy
> 650 to 1,500> 80 to 200> 30 to 60> 4.2 to 8.4Industrial areas with high humidity and aggressive atmosphere and coastal atmosphere with high salt loadBuildings or areas with almost continuous condensation and with high levels of impurities
C X
extreme
> 1,500 to 5,500> 200 to 700> 60 to 180> 8.4 to 25Offshore areas with high salt load and industrial areas with extreme humidity and aggressive atmosphere, as well as subtropical and tropical atmospheresIndustrial areas with extreme humidity and aggressive atmosphere

Typical environments and recommended surfaces/materials

Zinc removal: < 0.1 µm/a

Examples of typical environments

Open air 
–

Interior
 Heated building with neutral atmosphere

Recommended surfaces/materials

Electrogalvanised (G)

Layer thickness: 2.5 to 10 µm

Meeting room

Zinc removal: > 0.1 to 0.7 µm/a

Examples of typical environments

Open air 
Atmosphere with low degree of impurity

Interior
Unheated buildings, in which condensation can occur

Recommended surfaces/materials

Strip galvanised (FS)/zinc-aluminium alloy (DD)

Layer thickness: approx. 20 µm

High-rack warehouse

Zinc removal: > 0.7 to 2.0 µm/a

Examples of typical environments

Open air 
Urban and industrial atmosphere with medium sulphur dioxide load

Interior
Production rooms with high humidity and a certain amount of air impurity

Recommended surfaces/materials

Hot-dip galvanised (FT)/stainless steel A2

Layer thickness: approx. 40 to 60 µm

Building Industry

Zinc removal: 2.0 to 4.0 µm/a

Examples of typical environments

Open air 
Industrial atmosphere and coastal atmosphere with medium salt load, shipyards near the coast

Interior
Chemical plants, shipyards near the coast

Recommended surfaces/materials

Stainless steel A2

Rustproof

Building in the Food Industry: Smoking Oven

Zinc removal: 4.0 to 8.0 µm/a

Examples of typical environments

Open air 
Industrial areas with high humidity and aggressive atmosphere and coastal atmosphere with high salt load

Interior
Buildings or areas with almost continuous condensation

Recommended surfaces/materials

Stainless steel A4

Approved acid-resistant

Refinery Building

Zinc removal: 8.0 to 25 µm/a

Examples of typical environments

Open air 
Offshore areas with high salt load and industrial area with extreme humidity

Interior
Industrial areas with extreme humidity and aggressive atmosphere

Recommended surfaces/materials

Stainless steel A5

Approved high resistance

Industrial Buildings

Contact

OBO Bettermann Export GmbH & Co. KG

Do you have any questions on this topic? We are glad to help!