Fire protection competence

 

The basis for our comprehensive fire protection competence is a unique, very diverse product range. It makes us one of the few providers with a product range which covers all important protection aims of construction fire protection:

1. Limiting the spread of the fire,

2. Protect escape and rescue routes,

3. Maintaining the function of important electrical systems.

With OBO systems, planners and operators have the perfect components for the complete fire protection and function maintenance of their building.

Fire in the office

1st protection aim

Maintenance of the fire sections

The division of building into fire sections protects unaffected areas of the building from the spread of fire for specified periods of time.Insulation maintains the fire sections, thus limiting the spread of fire and smoke. These constructive measures protect people and property, allowing fire brigades to prevent the spread of fires to other parts of the building through extinguishing measures.

Function of firewalls

Fire walls should ensure that a fire cannot pass to neighbouring buildings or building sections. This creates so-called fire sections. The construction design of these firewalls (materials, fire resistance classes, stress values) is regulated by the building regulations and standards. Electrical cables and pipes may only be run through walls and ceilings at the ends of rooms when there is a guarantee that they do not present an opportunity for fire and smoke to spread.Insulation systems reliably seal the ceiling and wall penetrations required for installations against fire and smoke.

Fire walls
Partitioning systems
Partitioning systems
Partitioning systems
Partitioning systems

2nd protection aim

Protection of escape routes

According to the building regulations, there must be routes in buildings, which not only permit access to the building in a horizontal and vertical direction in normal situations, but which also offer the option of rescue in case of fire. It is therefore obligatory to equip buildings with at least one constructive emergency and escape route. Additional escape and rescue routes may also be necessary, depending on the type of building.

These include:

  • Necessary staircases (vertical access)
  • Connecting rooms between the necessary stairwells and exits to the outside
  • Necessary corridors (horizontal access)

There must be a guarantee that, if there is a fire, these routes can be used to leave the building without any risk. In addition to evacuation, the escape and rescue routes also aid the local fire brigades as a point of attack. In the area of emergency and escape routes, an installation must not pose an additional fire load. This requirement can be fulfilled using an appropriate type of installation:

  • Concealed installation
  • Installation in fire protection duct systems
  • Installation above suspended fire protection ceilings
  • Use of non-combustible materials
  • Routing of cables with improved behaviour in case of fire
suspended ceiling
Securing escape routes Installation method
Securing escape routes Installation method
Cable wrap

3rd protection aim

Maintaining the functionality of electrical systems

If there is a fire, emergency and escape routes must remain usable and important technical equipment, such as emergency lighting, fire alarm systems and smoke extraction systems, must continue to function. Therefore, it is essential that the power supply for these systems is specially protected. In addition, certain technical systems must support the fire brigades in fighting fires for a sufficiently long period of time.

Where is the maintenance of electrical function required?

Technical equipment with function maintenance is required for the following buildings and areas: Hospitals, hotels and restaurants, tower blocks, meeting places, shops, closed indoor car parks, metro systems, the chemical industry, power stations and tunnels.

This could be because these structures are regularly frequented by many people. This creates an increased safety risk for gatherings of people. However, with certain systems, property and the environment must also be protected.

Maintenance of electrical systems
Maintenance of electrical systems
Maintenance of electrical systems
Maintenance of electrical systems