Redefining sustainability: OBO EcoLine sets benchmarks in electrical installation

With OBO EcoLine, we have taken another step towards a more sustainable future. Our mission is clear: maximum carbon reduction, without compromising on quality, safety or functionality.
Cable support systems made from carbon-reduced steel, as well as clever connection and fastening solutions made from recycled materials, set new benchmarks in resource-efficient construction. The sustainable product variants are not only available as individual articles, but represent an extensive portfolio alongside the standard line. All products from the OBO EcoLine portfolio feature a higher proportion of recycled material or currently achieve carbon savings of at least 40% compared to the standard material.
Especially practical: The products from OBO EcoLine are fully compatible with existing systems. For planners and installers, that means no additional effort or adjustments are required.
With EcoLine, OBO impressively shows how proven system quality can be combined with sustainable innovation – setting a strong signal for the future of electrical installation.