The new Quick pipe fittings
For flexible installations and retroinstallations

Quick pipe is the intelligent system for flush-mounted installations and retroinstallations from the OBO product range. The system becomes particularly flexible and user-friendly through a selection of perfectly matched fittings. These have been optimised once again and stand out through countless advantages with regard to the construction and installation options. The Quick pipe fittings include: The T piece, the connection sleeve and the 90° bend.
All Quick pipe fittings are available in the four metric sizes M16, M20, M25 and M32. They can be opened and closed again without tools and stand out particularly on account of the fact they can accept corrugated pipes in addition to Quick pipe electrical installation pipes. These are held securely by an integrated rib contour in the interior of the fittings. The fittings can be installed in interior areas and protected exterior areas and can be used in the temperature range between –25 and +60 °C. The halogen-free material of the Quick pipe fittings offers increased safety by preventing the creation of any toxic gases in the event of fire.
Optimised portfolio stands out through countless benefits
One change to the Quick pipe fittings can be seen immediately: The T piece, which used to comprise two half shells, has been connected into a single component using an optimised hinge. The hinge can be easily opened and installed with just one hand. It can be opened and reclosed any number of times. This provides even more flexibility in terms of the installation and time savings as well, because there is no need to combine the two half shells. Retroinstallations can also be performed simply and any number of times.
The Quick pipe connection sleeve connects Quick pipe electrical installation pipes and corrugated pipes quickly and reliably. It allows a straight connection of two pipes. With its special shape, the 90° Quick pipe bend is ideal for internal and external corner installations. It guarantees right-angled routing of the pipes. The connection sleeve and the 90° bend also possess an optimised hinge, which can be opened easily, offering simple installation.
All the Quick pipe fittings have a protection rating of IP44 according to DIN EN 50529 and are VDE-certified according to DIN EN 50085.