News about OBO
What's new at OBO?
The Delta-Push® has set new standards in plug technology. It is easy to install, provides a secure hold and allows flexible use, while standing out with high extraction values in a variety of...
Anyone driving through the Menden-Hüingsen can hardly miss it: OBO is building a new logistics centre here right next to the metal competence centre on an area the size of four soccer pitches and is...
With the OBO floor trunking it is easy to route cables via the floor – and it’s ideal for the final few metres leading to the workstation.
The edge protection rings of the LKM wiring trunking system have been optimised and redesigned once again, and now offer the benefit of easy retrofitting. They can even be installed when the trunking...
Since 2019 the headquarter of OBO Finland can be found near the Finnish capital Helsinki. It consists of a sales company and a logistic site. When the Finnish colleagues moved to their new site, they...
An exciting event is on the horizon – from 3 to 8 March the Light + Building trade fair will again attract tens of thousands of international visitors to Frankfurt am Main. This industry highlight...
With numerous clever product details, the OBO flush-mounted and cavity wall boxes are setting new standards on every construction site in terms of quality and speed.
Some 400 children are educated here and receive basic education for a period of eight years. Medical clinics, therapy and care facilities are also an integral part of the school.
It was the summer of 2021 when OBO received a cry for help from the Andes: The Diospi Suyana mission hospital needed urgent support.
Ansgar Frommeyer from the aid organisation "Rolling Hospital" had a simple yet brilliant idea for supporting the Ukrainian civilian population: He converted a total of 12 buses into mobile warm rooms.