OBO BSSpro V1.1
Výrobky Systémová řešení Downloads Servis Novinky Projekty & Reference
Vítejte u OBO OBO BETTERMANN Slovensko OBO ve světě
obo-bettermann.com
Sitemap Kontakt
zpět


      BSS Fire protection systems

OBO BSSpro

From now on it is very easy to calculate the necessary material for different fire stop systems: With ?OBO BSSpro? all parameters can be find out easily.

The spreadsheets are easy to use and need no additional comments. You can start by clicking on any seal on the picture, to get right to the system, or with a click on the matrix-button .

Quick-info already show the names of the fire stop systems (picture 1).


Picture 1: Quick-Start with a system?s overview

You can choose the right system by checking several applications in the matrix. If you have made a choice, just click on the picto below to get to the calculation-spreadsheet of the system (picture 2). The seals for flushfloor- and screed-covered systems are already integrated as well as the tube seal CRM.


Picture 2: Matrix with all applications

All spreadsheets contain blue-layer input cells, brown cells for information and green cells with the results. Data can only be filled in the blue cells, all the others are protected. Deletion or manipulation of formulas etc. is not possible.

The entered values are checked. If you have entered a not permissible value, an alert-box will give a hint to correct the data (picture 3).


Picture 3: Alert-box

According to each seal, you can enter values for openings rectangular, as a drilling or as a given area. A handful of data is necessary to calculate the material: amount of seals, dimensions and the occupation density.

More than this, a matrix to convert different areas from square-metre to square-centimetres and vice-versa is integrated. You can reach the page with click on this button: .

The following systems are part of program:

  • HSM
  • Tangit
  • KBK (no calculation: just adding of different sizes approximately)
  • KBK-K (no calculation: just adding of different sizes approximately)
  • FBA-B, S30, S90 and UFS
  • FBA-BK (LFS)
  • FBA-F /-S /-SR /-D (no calculation: detailed data)
  • FBA-2K (UFS)
  • FPS
  • CRM (no calculation: detailed data)


Picture 4: Example of a calculation-spreadsheet ? here HSM

The button ?components? gets you directly to all needed products of each system including the article-numbers. A hint for the use of the document-set is placed on every first systems-site.

Return to the graphical overview or to the matrix with all applications is possible with the buttons ?Home? or ?Application? on each system?s site at any time .


Picture 5: FPS-site with special-application-button

Special applications can be reached by clicking on the according-buttons: .

For example, the site with detailed data for the tube-seal ?CRM? is attainable with a click on ?CRM?. Back to the main system is possible at any time.
All special-application buttons have got QuickInfo?s.

The following special-button is configurated for quick internet access (if online):
This button allows a direct link to OBO?s internet-site with systems animations.
You will find the button on the matrix-site.

    

Download OBO BSSpro

Manual OBO BSSpro V1.1 D | pdf | 933k


© 2004 OBO BETTERMANN GmbH & Co. KG - All rights reserved  | Kontakt | Tiráž | Vyloučení odpovědnosti | Ochrana dat | Autorská práva      O   O   O   O