OBO Consulidation Point, Deskbox, Flex duct
  
Products System solutions Downloads Service News Projects and References
Welcome to OBO OBO worldwide
obo-bettermann.com
Sitemap     Contact
back


        EGS Device systems

Consulidation Point, Deskbox, Flex duct
OBO Bettermann offers more flexibility in the office

Future-oriented workplace development – child’s play with the intelligent concepts from OBO Bettermann.

The engineer has less to do when it comes to planning office infrastructure. This is a move away from conventional installation, where excess cable around floor sockets was difficult to hide away well, patch cable was routed to the workplace without protection and it took a lot of effort to relocate fixed floor sockets.

All this is in the past – just like the separation of data, voice communication and power at the workplace. What we need today is integration into an extremely flexible overall solution.This is where the Bettermann range comes in: excess cable is stored in a false floor at the Consulidation Point. This point is the central position in the room, from which the workplace is supplied with power via Flex duct and the Deskbox. This means that the connection workplace. It is also much easier to relocate floor sockets.

The Flex duct is paving the way through new office landscapes for a highly functional and attractive type of cable routing. Individual elements can be combined or separated without any tools whatsoever. Rigid sections can be connected simply by clipping together, fixed areas can be pulled apart and moved again. Cables can also be retrospectively incorporated into the Flex duct.

The Deskbox can be equipped to your requirements with Modul 45 data and communication connections, sockets and switches. The Deskbox sets aesthetic benchmarks with its elegant shape and eight modern colours.

    


© 2006 OBO BETTERMANN GmbH & Co. - All rights reserved  | Contact | Imprint | Exclusion of liability | Data protection | Copyright      O   O   O   O