Staying flexible
The new WDK ducts with practical cover clip
The new cover clip greatly facilitates the fitting of OBO’s WDK ducts. The clip is continuously adjustable over the whole length of the duct. This means you can stay flexible and mobile during installation.
Another plus is the simplicity of cable insertion: the clip is locked in on one side and tilted forward. This gives a 30° opening, so that the cables can be laid in quickly and without problems. From a duct width of 100 mm the clip can also be used as a connector in the fitting of line routing ducts. When supplied the cover clip is attached to the bottom of the duct.
|