Overall solutions for tomorrow’s energy and data infrastructure
OBO BETTERMANN and Reichle & De-Massari
Infrastructure in motion
Changing economic conditions and new business models throws the working world into a state of real flux. This places a whole new set of demands on the office of the future. Permanent room structures are being superseded, optimised variability is a must. Office areas are being flexibly adapted to team size, reorganisations are the order of the day and relocation is becoming commonplace. Of course, this also affects the infrastructure in workplace development. Power supply and data networks are more mutually dependent. This has far-reaching consequences on how these infrastructures are planned, installed and operated. Overarching thinking and acting are gathering importance. OBO and R&M are entering into a partnership that will meet the challenges of these changes. Together, we will launch on the market a seamless, integrated solution for energy and data technology.
Modul 45 from OBO with R&M data technology
Modern offices are seeing a merging of networks. OBO solutions enable you to easily integrate highly sensitive PC electronics and communication devices into the standard switch installation. The coherent system that emerges is elegant, too because the data technology is harmonised with the Standard, Dialog, Aura and Modul 45 ranges. Maximum safety is guaranteed by OBO’s surge protection systems. They protect highly-sensitive, high-tech modules against voltage peaks. Cat. 5e connection modules of the R&M freenet cabling system are suitable for both voice and data applications. Cat. 5 connection modules are suitable for transmission frequencies of up to 100 MHz. Cat. 6 connection modules of the R&M freenet cabling system are suitable for voice, as well as fast data applications. Cat. 6 connection modules are suitable for transmission frequencies of up to 250 MHz. LWL connection modules can also be integrated. Everything fits into the system and can be altered as and when needed.
Connection module
Cat. 5e, unscreened |
Connection module
Cat. 5e, screened |
Connection module
Cat. 6, unscreened |
Connection module
Cat. 6, screened |
LWL
coupling
|
 |
 |
 |
 |
 |
 |
|
 |
|
 |
Flexible
No matter which connection modules you install: they all fit into the data technology module. Guaranteed by the standard size of the slide-in plate on the underside of the module. |
|
Future-proof
If the system is retrospectively changed, only the connection modules need to be replaced, the base carrier remains the same. |
|
Warranty
Assuming a construction using all components from R&M, we provide a 5-year warranty for products, a 20-year warranty for the system and a life-long warranty for the applications. |
The route to more protection
Eliminating integrity vulnerability around connectors is vital. Choose the R&M protection system for preventing network interruptions, errors, manipulations and other frequent error sources with a unique, simple yet intelligent solution.
The R&M protection system is set apart by its modularity and flexibility. It is based on Smartholes, which are integrated as standard into R&M platforms for copper and fibre-glass connectors. Plugs and switch fields therefore come prepared for the protection installation.
Convenient installation
Network protection is becoming increasingly important and a key factor for the future of entire organisations. Independent studies confirm that over 70% of network faults and crashes are down to incorrect cabling infrastructure and deliberate manipulation of the connection cables. Even when a passive cabling system is being evaluated, it is important to remember that the protection aspects can be integrally supported and implemented. The R&M protection system satisfies the diverse requirements and needs of the user.
Data meets power
The ability to quickly modify working environments to new needs and conditions hinges on having brand new office concepts. As the backbone of any modern office, the telephone, data and electrical infrastructure is gaining importance. In future, the cable infrastructure in false floors, suspended ceilings, telescopic columns and skirting ducts will form the technical basis for achieving the required flexibility at the workplace. In addition, infrastructures based on modular grids that are simple to expand are falling under increasing consideration. This means maximum flexibility with minimum costs for the company when it comes to relocating, reorganising or changing the use of office areas.
|