All OK
OBO rail and Flex duct
In the best way possible
A highly-functional and aesthetically appealing form of cable installation is making its way through the new office landscape: Flex duct from OBO is the ideal choice wherever cables need to be arranged and protected. Individual elements can be combined or separated without tools. Rigid sections can be produced by clipping together, fixed areas can be moved again by pulling apart. Cables can also be retrofitted into the Flex duct: simply push in.
Flex duct connection
The Flex duct can be extended or shortened and made rigid or movable without tools.
Good routing
The Flex duct protects the cable and routes in tidily from the wall or floor plug to the workstation.
Safety first
If installed overground, the duct is clicked into the ground track rail. This looks tidy and stops people tripping over exposed ducts.
Cable installation
The cables are inserted into the duct. The straps to the right and left of the duct are movable.
T-branch on the floor
A T-piece or connection to the device installation units enables the Flex duct to be arranged to the floor in a tidy manner.
|